This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMK04616EVM: LMK04616EVM

Part Number: LMK04616EVM

Tool/software: WEBENCH® Design Tools

Hi Ti !

I want to design the PLL2 loop filter with the TICS Pro software .I get phase marging of about 90 degree (in open loop) and can"t decrease it to values of 50-60 degree.How can I decrease the phase marging ?

is the PLL stable with that high value? can you advise ?

I set the following parameters:

  • Hi

    The PLL in LMK0461x devices is based on SDPLL architecture. The available settings for the intended bandwidth range are very stable settings. For sure, you can make it unstable. If you increase the integral gain settings and reduce the proportional gain settings, the PLL will get less stable.

    Here is one example setting:

    Please refer to the application note on the SDPLL operation.

    Best regards

    Puneet

  • Hi Puneet
    I have already make a design sourcing PLL2 with the local VCXO clock (122.88Mhz) ,PLL1 is bypass .I have get the output clocks frequency as i designed.I try to source PLL2 with CLKin1 (400Mhz @ +3  to 0dbm) using a divider of 2 in the REFCLK path but unfortunatly the PLL was unlock (as indicate by led D1) and there was no any output clocks .I performed the following sequence : reset the EVM then load the design,then click Device Start button .
    Can you advise what can be the problem .
    Thanks
    Yeshayahou

  • Hi Yeshayahou,
    Can you send me your TICSpro configuration file? You can save this by "File-Save" menu option.
    Best regards
    Puneet
  • Hello Yeshayahou,

    Please make sure that you have selected the correct clock (where you connect your input source) and the corresponding input is enabled.

    Also make sure that you select CLKin instead of OSCin from PLL2 page like shown below.

    If this does not solve you issue, then please send us the TICSpro config file for review.

    Best regards

    Puneet

  • Hi Puneet

    i tryed but ufortunatly still not work.see attach load file ,please change the file extention from txt to tcs .

    [SETUP]
    ADDRESS=888
    CLOCK=8
    DATA=4
    LE=2
    PART=LMK04616
    IFACE=SPI_CLKLOW
    ADDRESS_I2C=0x0
    
    [PINS]
    PINNAME00=SYNC
    LOCATION00=7
    PINVALUE00=False
    PINNAME01=RESETN
    LOCATION01=3
    PINVALUE01=True
    PINNAME02=CLKIN_SEL
    LOCATION02=1
    PINVALUE02=False
    
    [MODES]
    NAME00=R0
    VALUE00=126
    NAME01=R1
    VALUE01=511
    NAME02=R2
    VALUE02=767
    NAME03=R3
    VALUE03=768
    NAME04=R4
    VALUE04=1024
    NAME05=R5
    VALUE05=1535
    NAME06=R6
    VALUE06=1791
    NAME07=R8
    VALUE07=2303
    NAME08=R9
    VALUE08=2559
    NAME09=R10
    VALUE09=2815
    NAME10=R12
    VALUE10=3327
    NAME11=R13
    VALUE11=3583
    NAME12=R16
    VALUE12=4318
    NAME13=R18
    VALUE13=4862
    NAME14=R19
    VALUE14=5119
    NAME15=R20
    VALUE15=5184
    NAME16=R21
    VALUE16=5630
    NAME17=R22
    VALUE17=5711
    NAME18=R23
    VALUE18=6031
    NAME19=R24
    VALUE19=6289
    NAME20=R25
    VALUE20=6543
    NAME21=R26
    VALUE21=6796
    NAME22=R27
    VALUE22=7167
    NAME23=R28
    VALUE23=7423
    NAME24=R29
    VALUE24=7679
    NAME25=R30
    VALUE25=7935
    NAME26=R31
    VALUE26=8191
    NAME27=R32
    VALUE27=8447
    NAME28=R33
    VALUE28=8703
    NAME29=R34
    VALUE29=8959
    NAME30=R35
    VALUE30=8980
    NAME31=R36
    VALUE31=9471
    NAME32=R37
    VALUE32=9492
    NAME33=R38
    VALUE33=9983
    NAME34=R39
    VALUE34=10004
    NAME35=R40
    VALUE35=10495
    NAME36=R41
    VALUE36=10516
    NAME37=R42
    VALUE37=11007
    NAME38=R43
    VALUE38=11232
    NAME39=R44
    VALUE39=11311
    NAME40=R45
    VALUE40=11744
    NAME41=R46
    VALUE41=12020
    NAME42=R47
    VALUE42=12156
    NAME43=R48
    VALUE43=12308
    NAME44=R49
    VALUE44=12572
    NAME45=R50
    VALUE45=12800
    NAME46=R51
    VALUE46=13208
    NAME47=R52
    VALUE47=13411
    NAME48=R53
    VALUE48=13720
    NAME49=R54
    VALUE49=13923
    NAME50=R55
    VALUE50=14232
    NAME51=R56
    VALUE51=14435
    NAME52=R57
    VALUE52=14744
    NAME53=R58
    VALUE53=14947
    NAME54=R59
    VALUE54=15256
    NAME55=R60
    VALUE55=15459
    NAME56=R61
    VALUE56=15768
    NAME57=R62
    VALUE57=15971
    NAME58=R63
    VALUE58=16280
    NAME59=R64
    VALUE59=16483
    NAME60=R65
    VALUE60=16792
    NAME61=R66
    VALUE61=16995
    NAME62=R67
    VALUE62=17152
    NAME63=R68
    VALUE63=17448
    NAME64=R69
    VALUE64=17664
    NAME65=R70
    VALUE65=17940
    NAME66=R71
    VALUE66=18176
    NAME67=R72
    VALUE67=18437
    NAME68=R73
    VALUE68=18688
    NAME69=R74
    VALUE69=18964
    NAME70=R75
    VALUE70=19200
    NAME71=R76
    VALUE71=19496
    NAME72=R77
    VALUE72=19712
    NAME73=R78
    VALUE73=20048
    NAME74=R79
    VALUE74=20224
    NAME75=R80
    VALUE75=20640
    NAME76=R81
    VALUE76=20736
    NAME77=R82
    VALUE77=21152
    NAME78=R83
    VALUE78=21248
    NAME79=R84
    VALUE79=21759
    NAME80=R85
    VALUE80=21979
    NAME81=R86
    VALUE81=22261
    NAME82=R87
    VALUE82=22527
    NAME83=R88
    VALUE83=22783
    NAME84=R89
    VALUE84=23039
    NAME85=R90
    VALUE85=23295
    NAME86=R91
    VALUE86=23551
    NAME87=R92
    VALUE87=23566
    NAME88=R93
    VALUE88=24063
    NAME89=R94
    VALUE89=24319
    NAME90=R95
    VALUE90=24575
    NAME91=R96
    VALUE91=24831
    NAME92=R97
    VALUE92=25087
    NAME93=R98
    VALUE93=25343
    NAME94=R99
    VALUE94=25599
    NAME95=R100
    VALUE95=25855
    NAME96=R101
    VALUE96=26111
    NAME97=R102
    VALUE97=26367
    NAME98=R103
    VALUE98=26623
    NAME99=R104
    VALUE99=26879
    NAME100=R105
    VALUE100=27135
    NAME101=R106
    VALUE101=27391
    NAME102=R107
    VALUE102=27647
    NAME103=R108
    VALUE103=27889
    NAME104=R109
    VALUE104=27997
    NAME105=R110
    VALUE105=28191
    NAME106=R111
    VALUE106=28665
    NAME107=R112
    VALUE107=28927
    NAME108=R113
    VALUE108=29183
    NAME109=R114
    VALUE109=29191
    NAME110=R115
    VALUE110=29440
    NAME111=R116
    VALUE111=29706
    NAME112=R117
    VALUE112=29952
    NAME113=R118
    VALUE113=30210
    NAME114=R119
    VALUE114=30464
    NAME115=R120
    VALUE115=30751
    NAME116=R121
    VALUE116=31231
    NAME117=R122
    VALUE117=31487
    NAME118=R123
    VALUE118=31743
    NAME119=R124
    VALUE119=31999
    NAME120=R125
    VALUE120=32192
    NAME121=R126
    VALUE121=32448
    NAME122=R127
    VALUE122=32765
    NAME123=R128
    VALUE123=33023
    NAME124=R129
    VALUE124=33279
    NAME125=R130
    VALUE125=33535
    NAME126=R131
    VALUE126=33791
    NAME127=R132
    VALUE127=34047
    NAME128=R133
    VALUE128=34303
    NAME129=R134
    VALUE129=34367
    NAME130=R135
    VALUE130=34560
    NAME131=R136
    VALUE131=34816
    NAME132=R137
    VALUE132=35077
    NAME133=R138
    VALUE133=35328
    NAME134=R139
    VALUE134=35584
    NAME135=R140
    VALUE135=35852
    NAME136=R141
    VALUE136=36351
    NAME137=R142
    VALUE137=36607
    NAME138=R143
    VALUE138=36863
    NAME139=R144
    VALUE139=37119
    NAME140=R145
    VALUE140=37375
    NAME141=R146
    VALUE141=37602
    NAME142=R147
    VALUE142=37873
    NAME143=R148
    VALUE143=37892
    NAME144=R149
    VALUE144=38399
    NAME145=R150
    VALUE145=38655
    NAME146=R151
    VALUE146=38799
    NAME147=R152
    VALUE147=39055
    NAME148=R153
    VALUE148=39423
    NAME149=R155
    VALUE149=39935
    NAME150=R156
    VALUE150=40191
    NAME151=R157
    VALUE151=40447
    NAME152=R158
    VALUE152=40703
    NAME153=R159
    VALUE153=40959
    NAME154=R160
    VALUE154=41215
    NAME155=R161
    VALUE155=41471
    NAME156=R162
    VALUE156=41727
    NAME157=R163
    VALUE157=41983
    NAME158=R164
    VALUE158=42239
    NAME159=R165
    VALUE159=42495
    NAME160=R166
    VALUE160=42751
    NAME161=R167
    VALUE161=43007
    NAME162=R168
    VALUE162=43263
    NAME163=R169
    VALUE163=43519
    NAME164=R170
    VALUE164=43775
    NAME165=R171
    VALUE165=44031
    NAME166=R172
    VALUE166=44159
    NAME167=R173
    VALUE167=44539
    NAME168=R174
    VALUE168=44799
    NAME169=R175
    VALUE169=45055
    NAME170=R176
    VALUE170=45311
    NAME171=R177
    VALUE171=45567
    NAME172=R178
    VALUE172=45823
    NAME173=R179
    VALUE173=46079
    NAME174=R180
    VALUE174=46335
    NAME175=R181
    VALUE175=46591
    NAME176=R182
    VALUE176=46847
    NAME177=R183
    VALUE177=47103
    NAME178=R184
    VALUE178=47359
    NAME179=R185
    VALUE179=47615
    NAME180=R186
    VALUE180=47871
    NAME181=R187
    VALUE181=48127
    NAME182=R188
    VALUE182=48383
    NAME183=R189
    VALUE183=48639
    NAME184=R190
    VALUE184=48895
    NAME185=R191
    VALUE185=49151
    NAME186=R192
    VALUE186=49407
    NAME187=R193
    VALUE187=49663
    NAME188=R194
    VALUE188=49919
    NAME189=R195
    VALUE189=50175
    NAME190=R196
    VALUE190=50431
    NAME191=R197
    VALUE191=50687
    NAME192=R198
    VALUE192=50943
    NAME193=R199
    VALUE193=51199
    NAME194=R200
    VALUE194=51455
    NAME195=R201
    VALUE195=51711
    NAME196=R202
    VALUE196=51967
    NAME197=R203
    VALUE197=52223
    NAME198=R204
    VALUE198=52479
    NAME199=R205
    VALUE199=52735
    NAME200=R206
    VALUE200=52991
    NAME201=R207
    VALUE201=53247
    NAME202=R208
    VALUE202=53503
    NAME203=R209
    VALUE203=53759
    NAME204=R210
    VALUE204=54015
    NAME205=R211
    VALUE205=54271
    NAME206=R212
    VALUE206=54527
    NAME207=R213
    VALUE207=54783
    NAME208=R214
    VALUE208=55039
    NAME209=R215
    VALUE209=55295
    NAME210=R216
    VALUE210=55551
    NAME211=R217
    VALUE211=55807
    NAME212=R218
    VALUE212=56063
    NAME213=R219
    VALUE213=56319
    NAME214=R220
    VALUE214=56575
    NAME215=R221
    VALUE215=56831
    NAME216=R222
    VALUE216=57087
    NAME217=R223
    VALUE217=57343
    NAME218=R224
    VALUE218=57599
    NAME219=R225
    VALUE219=57855
    NAME220=R226
    VALUE220=58111
    NAME221=R227
    VALUE221=58367
    NAME222=R228
    VALUE222=58623
    NAME223=R229
    VALUE223=58879
    NAME224=R230
    VALUE224=59135
    NAME225=R231
    VALUE225=59391
    NAME226=R232
    VALUE226=59647
    NAME227=R233
    VALUE227=59903
    NAME228=R234
    VALUE228=60159
    NAME229=R235
    VALUE229=60415
    NAME230=R236
    VALUE230=60671
    NAME231=R237
    VALUE231=60927
    NAME232=R238
    VALUE232=61183
    NAME233=R239
    VALUE233=61439
    NAME234=R240
    VALUE234=61695
    NAME235=R241
    VALUE235=61951
    NAME236=R242
    VALUE236=62207
    NAME237=R243
    VALUE237=62463
    NAME238=R244
    VALUE238=62719
    NAME239=R245
    VALUE239=62975
    NAME240=R246
    VALUE240=63231
    NAME241=R247
    VALUE241=63487
    NAME242=R248
    VALUE242=63743
    NAME243=R249
    VALUE243=63999
    NAME244=R250
    VALUE244=64255
    NAME245=R252
    VALUE245=64640
    NAME246=R253
    VALUE246=64768
    NAME247=R254
    VALUE247=65152
    NAME248=R255
    VALUE248=65280
    NAME249=R256
    VALUE249=65664
    NAME250=R257
    VALUE250=65792
    NAME251=R258
    VALUE251=66176
    NAME252=R259
    VALUE252=66304
    NAME253=R260
    VALUE253=66688
    NAME254=R261
    VALUE254=66816
    NAME255=R262
    VALUE255=67200
    NAME256=R263
    VALUE256=67328
    NAME257=R264
    VALUE257=67712
    NAME258=R265
    VALUE258=67840
    NAME259=R266
    VALUE259=68224
    NAME260=R267
    VALUE260=68352
    NAME261=R268
    VALUE261=68861
    NAME262=R269
    VALUE262=69117
    NAME263=R270
    VALUE263=69373
    NAME264=R271
    VALUE264=69629
    NAME265=R272
    VALUE265=69885
    NAME266=R273
    VALUE266=70141
    NAME267=R274
    VALUE267=70397
    NAME268=R275
    VALUE268=70653
    NAME269=R276
    VALUE269=70909
    NAME270=R277
    VALUE270=71165
    NAME271=R278
    VALUE271=71421
    NAME272=R279
    VALUE272=71677
    NAME273=R280
    VALUE273=71933
    NAME274=R281
    VALUE274=72189
    NAME275=R282
    VALUE275=72445
    NAME276=R283
    VALUE276=72701
    NAME277=R284
    VALUE277=72959
    NAME278=R285
    VALUE278=73215
    NAME279=R286
    VALUE279=73471
    NAME280=R287
    VALUE280=73727
    NAME281=R288
    VALUE281=73983
    NAME282=R289
    VALUE282=74239
    NAME283=R290
    VALUE283=74495
    NAME284=R291
    VALUE284=74751
    NAME285=R292
    VALUE285=75007
    NAME286=R293
    VALUE286=75263
    NAME287=R294
    VALUE287=75519
    NAME288=R295
    VALUE288=75744
    NAME289=R296
    VALUE289=76000
    NAME290=R297
    VALUE290=76256
    NAME291=R298
    VALUE291=76512
    NAME292=R299
    VALUE292=76768
    NAME293=R300
    VALUE293=77024
    NAME294=R301
    VALUE294=77280
    NAME295=R302
    VALUE295=77536
    NAME296=R303
    VALUE296=77823
    NAME297=R304
    VALUE297=78079
    NAME298=R305
    VALUE298=78335
    NAME299=R306
    VALUE299=78591
    NAME300=R307
    VALUE300=78847
    NAME301=R308
    VALUE301=79103
    NAME302=R309
    VALUE302=79359
    NAME303=R310
    VALUE303=79615
    NAME304=R311
    VALUE304=79871
    NAME305=R312
    VALUE305=80127
    NAME306=R313
    VALUE306=80383
    NAME307=R314
    VALUE307=80639
    NAME308=R315
    VALUE308=80895
    NAME309=R316
    VALUE309=81151
    NAME310=R317
    VALUE310=81407
    NAME311=R318
    VALUE311=81663
    NAME312=R319
    VALUE312=81919
    NAME313=R320
    VALUE313=82175
    NAME314=R321
    VALUE314=82431
    NAME315=R322
    VALUE315=82687
    NAME316=R323
    VALUE316=82926
    NAME317=R324
    VALUE317=83199
    NAME318=R325
    VALUE318=83455
    NAME319=R326
    VALUE319=83596
    NAME320=R327
    VALUE320=83967
    NAME321=R328
    VALUE321=84223
    NAME322=R329
    VALUE322=84464
    NAME323=R330
    VALUE323=84735
    NAME324=R331
    VALUE324=84736
    NAME325=R332
    VALUE325=84992
    NAME326=R334
    VALUE326=85504
    NAME327=R335
    VALUE327=86015
    NAME328=R336
    VALUE328=86256
    NAME329=R337
    VALUE329=86524
    NAME330=R338
    VALUE330=86783
    NAME331=R339
    VALUE331=87008
    NAME332=R17
    VALUE332=4606
    
    [FLEX]
    FLOW_MODE_BYP1=Bypass 1
    FLOW_MODE_BYP2A=Bypass 2A
    FLOW_MODE_BYP2B=Bypass 2B
    FLOW_MODE_CPSL2O=Single Loop PLL2
    FLOW_MODE_CPSL2P=Single Loop PLL2
    FLOW_MODE_OPSL2O=Single Loop PLL2
    FLOW_MODE_OPSL2P=Single Loop PLL2
    FLOW_MODE_PDLO=Dual Loop
    FLOW_MODE_PDLP=Dual Loop
    FLOW_MODE_PSL1O=Single Loop PLL1
    FLOW_MODE_PSL1P=Single Loop PLL1
    BTN_DEV_STARTUP=BTN_DEV_STARTUP
    BTN_GET_SILICON=BTN_GET_SILICON
    BTN_GET_STATUS=BTN_GET_STATUS
    BTN_SWRST=BTN_SWRST
    BTN_UPDATE_VERSION=BTN_UPDATE_VERSION
    TICS_VERSION=1.6.7.0, 04-Jan-18 INI:2017-03-01 PY:20170517
    TICS_VERSION_NOTE=File from an earlier device profile loaded. Would like like to update the TCS file?
    EVM_CLKin0_FREQ=1
    EVM_CLKin0_SE=1
    EVM_CLKin1_FREQ=409.6
    EVM_CLKin1_SE=1
    EVM_CLKin2_FREQ=1
    EVM_CLKin2_SE=0
    EVM_CLKin3_FREQ=1
    EVM_CLKin3_SE=1
    EVM_CLKout0_FREQ=51.2
    EVM_CLKout0_Info=HSDS
    EVM_CLKout10_FREQ=25.6
    EVM_CLKout10_Info=HSDS
    EVM_CLKout11_FREQ=25.6
    EVM_CLKout11_Info=HSDS
    EVM_CLKout12_FREQ=12.8
    EVM_CLKout12_Info=HSDS
    EVM_CLKout13_FREQ=12.8
    EVM_CLKout13_Info=HSDS
    EVM_CLKout14_FREQ=12.8
    EVM_CLKout14_Info=HSDS
    EVM_CLKout15_FREQ=12.8
    EVM_CLKout15_Info=HSDS
    EVM_CLKout1_FREQ=51.2
    EVM_CLKout1_Info=HSDS
    EVM_CLKout2_FREQ=102.4
    EVM_CLKout2_Info=HSDS
    EVM_CLKout3_FREQ=102.4
    EVM_CLKout3_Info=HSDS
    EVM_CLKout4_FREQ=409.6
    EVM_CLKout4_Info=HSDS
    EVM_CLKout5_FREQ=409.6
    EVM_CLKout5_Info=HSDS
    EVM_CLKout6_FREQ=102.4
    EVM_CLKout6_Info=HSDS
    EVM_CLKout7_FREQ=102.4
    EVM_CLKout7_Info=HSDS
    EVM_CLKout8_FREQ=51.2
    EVM_CLKout8_Info=HSDS
    EVM_CLKout9_FREQ=51.2
    EVM_CLKout9_Info=HSDS
    EVM_DEVICE_TOPMARK=LMK04616
    EVM_OSCin_FREQ=409.6
    EVM_OSCin_SE=1
    EVM_OSCout_Info=HSDS
    EVM_OSCout_freq=409.6
    BTN_GET_CLKMUX=BTN_GET_CLKMUX
    BTN_GET_STORAGE=Read Storagecell
    BTN_MAIL_LF1=0
    BTN_PLL1_NDIV_SWRST=RST
    BTN_PLL1_RDIV_SWRST=RST
    BTN_PLL1_SWRST=RST
    CLKIN0_FREQ=1
    CLKIN1_FREQ=409.6
    CLKIN2_FREQ=1
    CLKIN3_FREQ=1
    INPUT_CLKIN0_PLL1_RDIV=32771
    INPUT_CLKIN1_PLL1_RDIV=32771
    INPUT_CLKIN2_PLL1_RDIV=32771
    INPUT_CLKIN3_PLL1_RDIV=32771
    INPUT_PLL1_NDIV=32771
    PFDCLKIN0_freq=3.05147844130481E-05
    PFDCLKIN1_freq=0.0124988556955845
    PFDCLKIN2_freq=3.05147844130481E-05
    PFDCLKIN3_freq=3.05147844130481E-05
    PFDCLKIN_freq=0.0124988556955845
    PLL1_EN_TIE_LOWCNT=1
    PLL1_EN_TIE_LOWCNT_WARNING=Divider register values different. Please refer datasheet
    PLL1_STORAGE_CELL_7t0=0
    VCXOPLL1_FREQ=409.6
    BTN_GET_PINSEL_DIV=Read
    BTN_OSCOUT_SWRST=RST
    OSCOUT_DRV_CURR_HCSL=0
    OSCOUT_DRV_MODE1_TEXT=DRV_CURR
    OSCOUT_DRV_MODE2_TEXT=DRV_RLOAD
    OSCOUT_DRV_MODE3_TEXT=DRV_MUTE
    OSCOUT_DRV_MUTE_HCSL=0
    OSCOUT_DRV_MUTE_HCSL_OPEN=0
    OSCOUT_DRV_RLOAD_HCSL_16mA=0
    OSCOUT_DRV_RLOAD_HCSL_4mA=0
    OSCOUT_DRV_RLOAD_HCSL_6_8mA=0
    OSCOUT_PINSEL_DIV_VALUE=0
    BTN_GET_STATUS_HOLDOVER=BTN_GET_STATUS_HOLDOVER
    BTN_PLL1_HOLDOVERCNT_SWRST=RST
    BTN_PLL1_HOLDOVER_DLD_SWRST=RST
    BTN_PLL1_HOLDOVER_LOCKDET_SWRST=RST
    HOLDOVER_DLD_COPY=0
    HOLDOVER_ERROR=For a proper function, the Digital Clock must \nbe switched on.
    HOLDOVER_LOL_COPY=0
    HOLDOVER_LOS_COPY=0
    PLL1_HOLDOVER_MAX_CNT_SECONDS=20.97152
    PLL1_HOLDOVER_MAX_CNT_UNIT=2
    BTN_MAIL_LF2=Request Support @ TI
    BTN_PLL2_AC_REQ=RST
    BTN_PLL2_NDIV_SWRST=RST
    BTN_PLL2_SWRST=RST
    CLKIN_FREQ=409.6
    OUTCH_CH7_freq=0
    OUTCH_CH8_freq=0
    PFDPLL2_FREQ=204.8
    PLL2_CLKin_freq=409.6
    PLL2_DBL_COMBOBOX=4
    PLL2_STRG_INITVAL_PRESET=4
    VCOPLL2_FREQ=6144
    VCOPRESCPLL2_freq=2048
    VCXOPLL2_FREQ=409.6
    BTN_CH01_SWRST=RST
    BTN_CH01_SWRST_SHOW=RST
    BTN_CH1011_SWRST=RST
    BTN_CH1011_SWRST_SHOW=RST
    BTN_CH1213_SWRST=RST
    BTN_CH1213_SWRST_SHOW=RST
    BTN_CH1415_SWRST=RST
    BTN_CH1415_SWRST_SHOW=RST
    BTN_CH23_SWRST=RST
    BTN_CH23_SWRST_SHOW=RST
    BTN_CH45_SWRST=RST
    BTN_CH45_SWRST_SHOW=RST
    BTN_CH67_SWRST=RST
    BTN_CH67_SWRST_SHOW=RST
    BTN_CH89_SWRST=RST
    BTN_CH89_SWRST_SHOW=RST
    CHANNEL01=1
    CHANNEL1011=1
    CHANNEL1213=1
    CHANNEL1415=1
    CHANNEL23=1
    CHANNEL45=0
    CHANNEL67=1
    CHANNEL89=1
    CHANNEL_SELECT=2
    CLKout0_FREQ=51.2
    CLKout10_FREQ=25.6
    CLKout11_FREQ=25.6
    CLKout12_FREQ=12.8
    CLKout13_FREQ=12.8
    CLKout14_FREQ=12.8
    CLKout15_FREQ=12.8
    CLKout1_FREQ=51.2
    CLKout2_FREQ=102.4
    CLKout3_FREQ=102.4
    CLKout4_FREQ=409.6
    CLKout5_FREQ=409.6
    CLKout6_FREQ=102.4
    CLKout7_FREQ=102.4
    CLKout8_FREQ=51.2
    CLKout9_FREQ=51.2
    VCOPRESCBOT_freq=2048
    VCOPRESCTOP_freq=2048
    btnApplyToChannel=Apply to\n selected\n Channel
    SPI_SCL_EN_INSTAGE=2
    SPI_SCS_EN_INSTAGE=2
    SPI_SDIO_EN_INSTAGE=2
    PLL2_REF_STATCLK_DIV_COPY=0
    STATUS0_EN_INSTAGE=1
    STATUS0_OUTPUT_DATA=1
    STATUS1_EN_INSTAGE=1
    STATUS1_OUTPUT_DATA=0
    SYNC_EN_INSTAGE=2
    SYNC_OUTPUT_DATA=0
    CLKINSEL1_EN_INSTAGE=2
    BTN_LOAD_DEVICE=Load from Device
    BTN_PLL1_BW_APPLY=Apply to Device
    BTN_PLL1_FIND_BW=Find Bandwidth
    BTN_PLL1_PLOT_CL=Plot Close Loop
    BTN_PLL1_PLOT_OL=Plot Open Loop
    BTN_SUGGEST_PLL1=Find PLL1 Settings
    DEBUG_PR=0
    LF_CEXTR=0
    LF_ERROR_BOX=0
    LF_FND_BW=0
    LF_FVCXO=122.88
    LF_INPUT_F=122.88
    LF_INPUT_MODE=0
    LF_INTG=0
    LF_NDIV=100
    LF_PFD_F=0
    LF_PLL_BW=20
    LF_PROP=20
    LF_RDIV=100
    LF_VCXO_GAIN=3
    BTN_LOAD_DEVICE_PLL2=Load from Device
    BTN_PLL2_BW_APPLY=Apply to Device
    BTN_PLL2_FIND_BW=Find Bandwidth
    BTN_PLL2_PLOT_CL=Plot Close Loop
    BTN_PLL2_PLOT_OL=Plot Open Loop
    BTN_SUGGEST_PLL2=Find PLL2 Settings
    DEBUG_PR2=.
    DEBUG_PR3=0
    LF2_CFILT=0
    LF2_CPROP=0
    LF2_ERROR_BOX=Error in inputs. VCO frequency out of range.Please check your Inputs.
    LF2_FND_BW=430
    LF2_FTREE=2048
    LF2_FVCO=6144
    LF2_INPUT_F=409.6
    LF2_INPUT_MODE=3
    LF2_INTG=31
    LF2_NDIV=10
    LF2_PFD_F=204.8
    LF2_PLL_BW=500
    LF2_PRE=0
    LF2_PROP=7
    LF2_RDIV=2
    LF2_RFILT=0
    BTN_FREQ_CALC=Find Solution
    BTN_PLL_FREQ_GO=Select
    FREQ1=122.88
    FREQ2=122.88
    FREQ3=0
    FREQ4=0
    FREQ5=0
    FREQ6=0
    FREQ7=0
    FREQ8=0
    FREQ_CLKIN=122.88
    FREQ_VCXO=122.88
    F_CALC_ERROR=0
    PFD1_1=0
    PFD1_10=0
    PFD1_11=0
    PFD1_12=0
    PFD1_2=0
    PFD1_3=0
    PFD1_4=0
    PFD1_5=0
    PFD1_6=0
    PFD1_7=0
    PFD1_8=0
    PFD1_9=0
    PFD2_1=0
    PFD2_10=0
    PFD2_11=0
    PFD2_12=0
    PFD2_2=0
    PFD2_3=0
    PFD2_4=0
    PFD2_5=0
    PFD2_6=0
    PFD2_7=0
    PFD2_8=0
    PFD2_9=0
    S10NDIV1=0
    S10NDIV2=0
    S10PRE=0
    S10RDIV1=0
    S10RDIV2=0
    S10DBL=0
    S10RDIV2_4=0
    S11NDIV1=0
    S11NDIV2=0
    S11PRE=0
    S11RDIV1=0
    S11RDIV2=0
    S11DBL=0
    S12DBL=0
    S12NDIV1=0
    S12NDIV2=0
    S12PRE=0
    S12RDIV1=0
    S12RDIV2=0
    S1DBL=0
    S1NDIV1=0
    S1NDIV2=0
    S1PRE=0
    S1RDIV1=0
    S1RDIV2=0
    S2DBL=0
    S2NDIV1=0
    S2NDIV2=0
    S2PRE=0
    S2RDIV1=0
    S2RDIV2=0
    S3DBL=0
    S3NDIV1=0
    S3NDIV2=0
    S3PRE=0
    S3RDIV1=0
    S3RDIV2=0
    S4DBL=0
    S4NDIV1=0
    S4NDIV2=0
    S4PRE=0
    S4RDIV1=0
    S4RDIV1_2_0=0
    S4RDIV2=0
    S5DBL=0
    S5NDIV1=0
    S5NDIV2=0
    S5PRE=0
    S5RDIV1=0
    S5RDIV2=0
    S6DBL=0
    S6NDIV1=0
    S6NDIV2=0
    S6PRE=0
    S6RDIV1=0
    S6RDIV2=0
    S7DBL=0
    S7NDIV1=0
    S7NDIV2=0
    S7PRE=0
    S7RDIV1=0
    S7RDIV2=0
    S8DBL=0
    S8NDIV1=0
    S8NDIV2=0
    S8PRE=0
    S8RDIV1=0
    S8RDIV2=0
    S9DBL=0
    S9NDIV1=0
    S9NDIV2=0
    S9PRE=0
    S9RDIV1=0
    S9RDIV2=0
    SOL_SEL=0
    S_1=1
    S_10=10
    S_11=11
    S_12=12
    S_2=2
    S_3=3
    S_4=4
    S_5=5
    S_6=6
    S_7=7
    S_8=8
    S_9=9
    VCO_1=0
    VCO_10=0
    VCO_11=0
    VCO_12=0
    VCO_2=0
    VCO_3=0
    VCO_4=0
    VCO_5=0
    VCO_6=0
    VCO_7=0
    VCO_8=0
    VCO_9=0
    VCXO_1=0
    VCXO_10=0
    VCXO_11=0
    VCXO_12=0
    VCXO_2=0
    VCXO_3=0
    VCXO_4=0
    VCXO_5=0
    VCXO_6=0
    VCXO_7=0
    VCXO_8=0
    VCXO_9=0
    OSCIN_BUF_LOS_EN=0
    OSCIN_BUF_REF_EN=0
    OSCIN_BUF_TO_OSCOUT_EN=0
    OSCIN_OSCINSTAGE_EN=1
    OSCIN_PD_LDO=1
    OSCIN_SE_MODE=1
    

  • Hi

    I fixed your configuration. This should work.

    Best regards

    Puneet

    LMK04616_409p6_PLL2only.zip

  • Hi puneet
    Thanks it's works.
    I think that there is a bug in the GUI ,there is no a right frequency output from OSCOUT till toggling the OSCOUT_DIV select button and changing the the divide value.
    Thanks
    Yeshayahou
  • Hi Yeshayahou,
    Do you mean that you program the OSCout divider at device configuration and when you load the registers, you dont see a correct frequency unless you toggle the OSCout_DIV select button and change the divider values again?
    Once you change the divider values, you should also do OSCout divider reset.
    Best regards
    Puneet
  • Hi Puneet

    Yes,when i load the TCS program file with the OSCout divider option drived from PLL2 the was no any output .I change the divider by de-select and re-select it and then there was a signal output with correct  freqency.

    THANKS

    Yeshayahou

  • Hi Yeshayahou,
    I check now in the Lab and confirm that there is a bug in the software and I will fix that in the next release. For the time being, you can use the OSCOUT_SWRST button.
    Best regards
    Puneet