Part Number: LMK03318
HI,
I am using LMK03318 now, but there is no output.
I use an 10MHz oscillator as secondary reference input, doubler enable, M-divider set /2 ,VCO at 5000MHz ,and VCO out at 1000MHz, C2 is 33nF.
I need some 40MHz CMOS output so i set output-divider as 25.
But there is no output.
When i set clock source at secondary reference input, for example channel 5, i can see 10MHz output.
I think this problem maybe the wrong set of R2 R3 C1 C3,but not sure.
help me please.
Best regards!
Leon