Other Parts Discussed in Thread: LMX2592EVM, LMX2592,
Hi Support,
Tested LMX2594 chip using LMX2592EVM, but the phase noise performance is inferior to LMX2592 chip.
Here are the details about the Ref and output frequency.
Reference to the chip: 50MHz (bliley 50MHz ocxo ,phase noise at 10KHz is -160dBc/Hz) ,used doubler inside the chip so the phase detector frequency is 100MHz.
Output frequency: 13.275 to 14.5 GHz (only 6 frequencies in this range)
Phase noise requirement: 10KHz@ -90dBc/Hz and 100KHz@-100dBc/Hz
FYI, Able to achieve the above phase noise LMX2592 chip (6db better since the outfrequency is half of the above mentioned).
In addition, what changes are required to use LMX2594 on LMX2592EVM?
Lastly, please help to advise the loopfilter values for out above frequency requirement.
Thanks.