Other Parts Discussed in Thread: LMX2491
Tool/software: WEBENCH® Design Tools
Hello.
I am attempting to use the 2492 as a FMCW frequency source controlling a VCO in a saw tooth pattern from 300MHz to 700MHz. The device is advertised to work from 500MHZ, but I am able to get it to work down to 400MHz. Can you suggest an alternate synthesizer chip to use? Do you think I could lock using the second harmonic? ie 600MHz through 1400MHz?
Thanks very much for your help.
Jim
858 204 9422