Other Parts Discussed in Thread: LMK61E2, TIDA-00626
respected,
i have been working on reference design TIDA-00626. which consist of on board oscillator option as well as LMK61e2 option. i have by passed the resistors to disconnect LMK61e2 from the board and prefer using the fixed frequency oscillator. what will be the efficiency of using on board oscillator rather than using LMK61E2. also how we can test that whether we are getting 100 MHz signal from the oscillator pin. can it be tested on DSO or spectrum analyser.