Part Number: LMX2492EVM
Hello,
I use the LMX2492EVM and TICS PRO to generate a chirp composed by two ramps :
- RAMP0 : 9300 --> 9350 MHz during 100 us, then,
- RAMP1 : 9350 --> 9400 MHz during 600 us, then,
- RAMP0 etc.
I use the TRIG1 pin to output RAMP0 state (+V active; 0V inactive).
As expected, the TRIG1 pin generate +V during 100 us and then 0V during the next 600 us.
But when i check the DLY function on RAMP1, i don't have expected ramp profil on TRIG1 pin : +V during 100 us and then 0V during the next 1,2 ms.
Can somebody could explain me this function DLY ?
Thank you in advance,
Regards,
Guillaume Motyl