Part Number: LMX2582
Other Parts Discussed in Thread: LMX2571, LMX2581, LMX2485E, LMX2572
I want to sweep a PLL VCO from 50MHz to 90MHz.
Instrumentation type application.
Frequency of Phase Detector probably 100MHz.
For Ref Frequency Input - I prefer to use 10MHz TXCO but will consider 20MHz crystal.
The LMX2571 appears to be quite suitable.
But is the LMX2581 family vastly superior?
Is there more popular part I should consider?
Does TI have sub 20MHz - 100MHz active mixers that go well with these parts?
--------
The LMX2571 data sheet suggests you can step from one frequency to the next in about 1.5ms.
Is this just switching time between two pre-set Frequencies.
Or is it the time that a new frequency can be entered, CALed and be stable.
So 1000 points could be swept in 1.5 seconds.
Thanks