Part Number: LMX2594
Dean,
I have a ramp that goes up then down 100 MHz with each leg taking 100us. This is a nice start. Now I want to have a signal that is synchronized with the 2594 clock to enable digitizing with an external A/D. Whenever I try to program the 2594 to do SYSREF_EN mode, it eventually disrupts my ramping. Here is a screen shot before I go to turn on VCO_PHASE_SYNC
Here is my setup when I get the synch signal SYSREF to work. It outputs a nice 14.375 MHz signal.
(Don't worry about the channel divider output. I only have an HP53310A modulation domain analyzer in order to look at the F vs T output, so I sometimes need to channel divide by 4, sometimes just by 2.)
How can I have a ramp output from the 2594 that I can synchronize against? Is the SysRef signal not the correct one to use?
Thanks,
Darren R