Part Number: LMK00105
Hi all
Would you mind if we ask LMK00105?
<Question1>
There is no recommended schematic in case of AC coupling with LVDS input.(Differential input)
If you have it. could you share it?
<Question2>
In relation to <Question1>, is it possible to configure termination resistor 100ohm after AC coupling?
Because we assume that there is the voltage difference 0.3V between CLKIN+ and CLKIN-.
<Question3>
We would like to confirm VCM of Electrical Characteristics on the datasheet.
We assume that VCM range will be small as the input is larger.
It seems that it is opposit. Is our recognition wrong?
Kind regards,
Hirtotaka Matsumoto