This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK61E2: CodeLoader

Part Number: LMK61E2
Other Parts Discussed in Thread: CODELOADER

I am looking for an easy way to configure the LMK61E2 oscillator and I came accross the CodeLoader v4.20.2.  It seem like CodeLoader support programming the LMK61E2, but when I look at the register map, it doesn't have all the registers specified in the LMK61E2 datasheet.  For example, register R3 and R10 isn't in the program.  Also, CodeLoader contain registers that isn't in the datasheet such as register R24. 

So my question is does CodeLoader support the LMK61E2?  If so, how do I map the register table from CodeLoader to the register table in the datasheet?  The datasheet only has 1 byte per register, but CodeLoader seem to contain at least 2 bytes.  Should I ignore the upper bytes?