Other Parts Discussed in Thread: TIDA-01410
Dear,
I did perform power measurments (LMX2594 EVM). The maximum output power doesn't reach my desired power level~ 6 to 7 dBm @ [9 to 11GHz]
According to what I red in this topic, many users got 1 to 2 dBm with a resistive load. I got the same level. The only way for me to figure out, is to use a 1nH inductor Pull-up. The issue is that I do not have a tuner to determine the output impedance in order to optimize the power transfert.
Do you have a file that provides the output impedance of the PLL (or the impedance that you find thanks to the tuner) ? If not, do you have any realized or simulated design (an output matching network) that has been used at these frequency range.
Thank you,