This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCV304: Ripple on the VDD pin

Part Number: CDCV304

HI, Team:

Do we have any requirment on the CDCV304PWR VDD pin ripple or noise to guarantee the output clock performance?

Thansk!

  • Hi Andrew,

    No special ripple requirements.
    CDCV304 can work in VDD range 2.3~3.6V, in this range, CDCV304 always can run.
    But power supply ripple frequency would be transferred to output spurs, and CDCV304 has no special PSRR design.
    So if customer like to achieve low jitter performance, ripple on VDD should be controlled, depends on clock jitter requirement.


    Regards,
    Shawn Han