Part Number: LMX2594
I have an custom board with several LMX2594's on it using a 100MHz reference and PFD, in integer mode, N=80, with a VCO frequency of 8000MHz, with RFOUT_A and RFOUT_B outputs configured for an output of 4000MHz, Register 75 / 0x4B = 0x0800 and register 0x1F = 0x03EC (or 0x43EC). this is stable and works fine!
From the manual, and the TICS Pro programs output, If I want to change the output frequency to 2000MHz, it looks like all I need to do is change the CHDIV value and possibly set the CHDIV_DIV2 bit?
When I do this, Register 75 / 0x4B = 0x0880, and register 31 / 0x1F = 0x43EC,I expect a 2000MHz output, but the output stays at 4000MHz,
I am using a custom board, so I can’t directly use TICS to talk to the board but my initial register load came straight out of TICS, and I am programming all 113 registers as recommended. (and the Same as TICS outputs) This happens the same on power-up as it does reloading all, or the two registers on a powered part.
Am I missing a register somewhere? To me it looks like the part won’t run with both outputs with a divider order greater than 2?
Respectfully
Rich