Part Number: CDCI6214EVM
Other Parts Discussed in Thread: TICSPRO-SW
I am trying to run the CDCI6214EVM board off of an external clock connected to the XIN port. I initially configured the board to run off the crystal at 10 MHz. But when a switch the reference from the crystal to LVCMOS and supply an external signal, there is no change in the board behavior and the board generated clock signal is not synchronized to the externally generate 10 MHz signal. All the frequencies I have set are multiples of 10 MHz so synchronization should be easy, but I am having no success.
Part of the problem is I do not know the proper format for the external clock. I am currently generating a 10 MHz square wave the varies between 0 V and 1.8 V, but the user guide provides me with very little guidance as to what I am supposed to apply.
How do you get this board to lock to an external clock?
Thanks for the help.