Part Number: CDCM7005
We have had to change the VCXO Vectron VX-705-ECE-KEAN-100M000000 used with the CDCM7005 due to a lack of stock and we have changed to the Abracon ASG-P-V-A-100.000MHz.
With the first one we don't have any problem to synvhronize. With the secon one we have important problems.
The problem identified is that the Texas CDCM7005 do not provide Control Voltage output until it has a signal at its input, and this signal it is not provided by the Abracon VCXO until it has Control voltage, producing a blocking situation (This did not happen with the Vectron VCXO because it provided always signal at its output).
We have initially solved this problem by using the Preset Charge Pump output voltage of the CDCM7005 which forces a voltage at the output of the Control Voltage. This allows the VCXO to start providing signal at its output. Removing this preset immediately, it is obtained, apparently, a way to break of the blocking status. Unfortunately, this methode do not always work, due to it is not controlable the timing of the process. Do you have any suggestion on the CDCM7005 control to solve the problem?