Other Parts Discussed in Thread: LMK00804B, LMK00725
We need to disable the output of a MAX3761 in an application which is sensitive to glitches. The disable of the MAX3761 isn't fast enough and produce glitches on the output. I'm interested in a clock buffer which supports glitch free clock interruption/disabling with a speed rate up to 500 MHz. Do you have any recommendation? We can't use any PLL solution as our clock changes non stop.