Part Number: LMX2594
Is there a way to adjust output power setting for simulations running in HyperLynx?
If not, what setting does the IBIS model default to (RESET = 31)?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Simon,
Has the IBIS model for LMX2594 at the TI website,
dated June 06 2017 been verified? The differential pin assignment for RFOUTB and RFOUTB* is reversed
18 RFOUTB RFOUT 0.04055 0.82255n 0.18102p
19 RFOUTB* RFOUT 0.04205 0.86548n 0.18126p
[Diff pin] inv_pin vdiff tdelay_typ tdelay_min tdelay_max
|
8 9 0. 1 NA NA NA
18 19 NA 0.0s 0.0s 0.0slmx2594.ibs