Part Number: LMX2582
Other Parts Discussed in Thread: USB2ANY
Dears,
I lost the communication between the TICS PRO and the LMX2582EVM. TICS PRO detects the board, but it can't write any register. The Board is consuming 0.17 A.
Any idea to resolve that problem?
How can I identify if the problem is from the USB2ANY or from the EVM it self.
It was working well, and suddenly I lost the communication.
Regards,