This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00301: Osc 100MHz input CLK_INP/N

Part Number: LMK00301

Hi there:

I'd like to check if using Osc to generate the 100MHz signal which could input to the CLKin 0/1 or not?  It since the crystal input (OSin could accept 10~40MHz only)

If it's not workable, what's suggestion to customer ?