Part Number: LMK04610
Other Parts Discussed in Thread: CDCLVP1102, , CDCLVC1102
Hi !
I design to connect a difference clock of 410Mhz to differential clock input pins OSCinp/n ,using only PLL2 .The clock is a sinus wave converted to differential wave by a transformer with 100 ohm termination, then AC couple .
Each input pin have a 1.3Vptp signal amplitude.
Should i have to protect the input pins from over amplitude voltage when device is un-power and the clock is active?
The datasheet require a maximum voltage of -0.3V to (VDD_IO+0.3) ,which give +-0.3V when un-power.
If the answer is positive then can you advise how to implement it?
Thanks
Yeshayahou