Part Number: CDCLVC1104
Hello
I have some questions about CDCLVC1104.
1.
The datasheet (SCAS895B) defines “Input slew rate” as 1 – 4 V/ns in 6.3 Recommended Operating Conditions table.
If input clock is slower than this definition like 0.4V/ns with 33MHz, what kind of problem could happen?
2.
The same datasheet recommends to use ferrite bead on the power supply in page 12 of 10 Power Supply Recommendations.
What kind of problem could happen if this ferrite bead is not used? The input clock frequency is the same, 33MHz.
Regards,
Oba