This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: Use two vcxo to this PLL chip ?

Part Number: LMK03318


Hi

   I would like to use two vcxo to supply for this chip , and using software to select one at one time , is there any problem ?

 By the way , in order to minimux the expensive , the two vcxo may be cheap price, so the jitter of the vcxo maybe not good , such as 100 ps rms . So if I make a narrow PLL band by using  LMK03318, can I get   the output  clock jitter  below 1ps or 100fs ? (the input and output frequency is 24M and  6M , actruely a divider) 

Thanks 

  • This device does not support external VCXO, as the both PLLs have integrated VCO which is the only option. The internal VCO could achieve < 1ps rms jitter (12k-20MHz integration bandwidth) with narrow loop bandwidth, but not 100 fs. The 100 fs spec assumes a low-jitter reference, such as XTAL input with the built-in XTAL oscillator input stage or low-noise XO source with less than 100 fs jitter.

    Alan