This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVD2102: Swaping inputs & outputs

Part Number: CDCLVD2102

Hello, can I swap the P/N inputs and outputs?
for example use INN0 as P input and INP0 as N input and then on the output also use OUTN as P output and OUTP as N output

As far as I understand this is possible but just want to make sure,

Thank you.