This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDC3RL02: Min spec of CLDO in datasheet

Part Number: CDC3RL02

Hi 

I am using 2.2uF X5R 6V3 20% ceramic capacitor on VLDO (pin B1).

At low temperature ~0deg C the LDO oscillates at ~ 1.2MHz causing 1.2MHz spurs on the CLK output.

I am certain the capacitance value remains above the minimum required value of 1uF at this temperature.

Is there any requirement for min or max ESR on the CLDO capacitor?

Thank you

Chris