Part Number: LMX2571
Hello,
I'm working with one of our customers and they have the following request:
"I’m testing synthesizer LMX2571 on evaluation board LMX2571EVM. I have some problem with 2FSK frequency deviation.
- What are relationships between frequency deviation for the 2FSK modulation scheme (the FSK modulating data pin FSK_D0 and the clock pin FSK_DV0 for FSK PIN mode are used) and registers R9 (FSK_DEV0_F1) and R10 (FSK_DEV1_F1)?
What should be settings for R9 and R10 e.g. for symmetrical 2FSK frequency deviation +-400 kHz?
- Also, I can’t find what LMX2571’s parameter is responsible for the modulation magnitude (scaling frequency deviation)?"
Thank you!
Regards,
Ryan B.