This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: Estimation Phase Noise and RMS Jitter

Part Number: CDCI6214

Hello, 

I have a question about CDCI6214.

[Q]

Could you estimate the output phase noise, RMS Jitter, under the following conditions?

(A)
- input : 50MHz (SG-210STF-50.0000MHZ)
 

0.1	-120.3325358
0.2	-128.3621199
0.3	-132.8279977
0.4	-135.8841525
0.5	-138.1892076
0.6	-140.0297579
0.7	-141.5554624
0.8	-142.8539681
0.9	-143.9808616
1	-144.9735357
2	-151.0538019
3	-154.0725129
4	-155.8437334
5	-156.9622227
6	-157.7036019
7	-158.214353
8	-158.5779657
9	-158.8443085
10	-159.0443123
20	-159.7448234
30	-159.8857755
40	-159.9359343
50	-159.9592807
60	-159.9719926
70	-159.9796661
80	-159.9846493
90	-159.9880667
100	-159.9905115
200	-159.9983284
300	-159.9997753
400	-160.0002815
500	-160.0005158
600	-160.000643
700	-160.0007197
800	-160.0007695
900	-160.0008037
1000	-160.0008281
2000	-160.0009061
3000	-160.0009206
4000	-160.0009256
5000	-160.000928
6000	-160.0009292
7000	-160.00093
8000	-160.0009305
9000	-160.0009308
10000	-160.0009311
20000	-160.0009319
30000	-160.000932
40000	-160.0009321
50000	-160.0009321
60000	-160.0009321
70000	-160.0009321
80000	-160.0009321
90000	-160.0009321
100000	-160.0009321
200000	-160.0009321
300000	-160.0009321
400000	-160.0009321
500000	-160.0009321
600000	-160.0009321
700000	-160.0009321
800000	-160.0009321
900000	-160.0009321
1000000	-160.0009321

- VCO : 2500MHz

- output : 156.25MHz(LVDS) RMS Jittter(Integrated BW = 12kHz to 20MHz) = ?
                125MHz(LVDS) RMS Jittter(Integrated BW = 12kHz to 20MHz) = ?
                100MHz(LVDS) RMS Jittter(Integrated BW = 12kHz to 20MHz) = ?

(B)
- input : 15.36MHz
 

10	-81.69040788
20	-87.71279393
30	-91.23521395
40	-93.73428534
50	-95.67266277
60	-97.25640492
70	-98.59542355
80	-99.7553237
90	-100.7784208
100	-101.693607
200	-107.7143331
300	-111.2361301
400	-113.7348118
500	-115.672872
600	-117.2563158
700	-118.595032
800	-119.7546141
900	-120.7773712
1000	-121.6921917
2000	-127.7075496
3000	-131.2206285
4000	-133.7071826
5000	-135.6297189
6000	-137.1942744
7000	-138.5107805
8000	-139.6448819
9000	-140.638946
10000	-141.5219266
12000	-143.0319562
20000	-147.0638401
30000	-149.8892022
40000	-151.5693357
50000	-152.6407914
60000	-153.3568107
70000	-153.8535303
80000	-154.2092594
90000	-154.4711531
100000	-154.6686719
200000	-155.3682288
300000	-155.5111187
400000	-155.5622619
500000	-155.5861393
600000	-155.5991651
700000	-155.6070381
800000	-155.6121556
900000	-155.6156677
1000000	-155.6181816
2000000	-155.6262292
3000000	-155.6277211
4000000	-155.6282434
5000000	-155.6284852
6000000	-155.6286165
7000000	-155.6286957
8000000	-155.6287471
9000000	-155.6287824
10000000	-155.6288076
20000000	-155.6288882

- VCO : 2457.6MHz

- output : 245.76MHz(LVDS) Phase Noise @ 10kHz = ? (Customer's target = -105.08678 dBc/Hz)
                                              Phase Noise @ 100kHz = ? (Customer's target = -125.08678 dBc/Hz)
                                              Phase Noise @ 1MHz = ? (Customer's target = -145.08678 dBc/Hz)

Best Regards,

Kaede Kudo