Part Number: LMX2582
Hello,
I'm using LMX2582 and I need to calculate the loop bandwidth.
How can I know the equations used by PLLatinum Sim to calculate the LBW? I referred to "PLL Performance, Simulation, and Design © 2017" Page 378 to calculate the open-loop and then the closed loop cutoff frequency, it differs from the one appeared in the PLLatinum Sim. I considered the Type of the filter used, Gain, R&C Values, input & output Frequencies, Kvco, CPGain, N...
Regards,