This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: How to use FCAL_EN?

Part Number: LMX2594


Hi,

after setting FCAL_EN='0' and then FCAL_EN="1" to perform the calibration, if I dont want to check anything anymore, should I return it to "0" for normal operation or to leave it at "1", and only if I will want to change the frequency I will toggle it again to "0" and then to "1" and leave it at "1"?

for short, after the calibration what should be the state of this bit (normal operation)?