Part Number: CDCM6208
Hi all.
I have two questions about CDCM6208.
1.I think that there is no power supply sequence in particular otherwise than the following.
Is it correct my understanding?
"It is necessary to ensure that device calibration occurs AFTER the DVDD supply as well as the VDD_PLL1, VDD_PLL2, VDD_PRI,
and VDD_SEC supply are all operational, and the voltage on each supply is higher than 1.45."
2.If device powered up normally, can we set register(for example output frequency) any time?
Best Regards,
Sho