Part Number: LMX2594
I am looking at the LMX2594 for a fixed frequency application. However, I have a few questions:
- Is a layer plot or cad files available for theLMX2594 EVM, eval board? I see them for the multiple PLL board, but the not the eval board I have.
- I am trying to minimize power draw so I have only 1 output turned on, however I need to distribute the signal to two different connectors. Can I use the RFOUTAM and RFOUTAP to drive two separate modules? I would assume these outputs are 180 deg out of phase and are meant to be combined to get a bit more power out. Are there concerns? Any idea what the isolation between these two outputs are? I am planning on biasing the outputs with the 18nH and 50 ohm resistor, per the datasheet.