This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: MUX Pin Behavior for Microwire Readback

Part Number: LMX2595

I intend to place 2x LMX2595 devices on a single microwire (SPI) bus.  My question is this:  Does the MUX pin, if configured for Microwire read back via a proper register write, go into a high impedance state when the LE line of the device is pulled high?  If so I can connect the MUX line for 2 or more devices onto the SPI bus MISO line and a singular device with LE pulled low will dictate the state of the MISO line, so long as all other devices on the SPI bus have their LE lines in a high state.

Many Thanks,

David