Part Number: LMX2595
Other Parts Discussed in Thread: LMX2571, LMX2572
Hi TI Experts,
My customer need an adjustable reference generator with good phase noise to remove the integer boundary spurs.
They need 200 MHz spur free bandwidth from the LMX2595. They are looking for a clean configurable clock so they can avoid crosstalk spur and IBS to get spur free performance across 200 MHz.
Detail requirements as below:
- Is this signal source for a mixer?
It will either be LO for mixer for modulated signal or direct to output stages as CW signal source.
- What frequency range?
10 MHz - 19 GHz
- What phase noise spec?
Phase noise is not the issue. We want to remove IBS, x-talk and other spurs. We found that we cannot do it with a fixed frequency clock. We're targetting 90 dBc SFDR across at least 200 MHz of usable bandwidth centered on the LO frequency. That being said, system phase noise should be ~ -90 dBc @10kHz.
- What reference will be used?
A 10 MHz external OXCO will be used as system clock.
Can TI please advice the suitable part in this case.
Thanks,
Br,
Teach Me