This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Bypass capacitors on Vbias & Vref pins

Part Number: LMX2594

Hi,

I wish to operate the LMX2594 with a100MHz input clock  and output frequency of 1408MHz.

Due to board space limitations I cannot comply with the requirements for 10uF capaitors on the Pins VREFVCO, VREFVCO2, VBIASVCO , VBIASVCO2, VBIASVARAC.

Instead I placed 1uF & 0.1uF adjacent to the pin.

Could you predict what would be the effect on the device performance?

Regards,

Itai