This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00105: Is the current linearly dependent on Vddo?

Part Number: LMK00105


Hi team,

In the LMK00105 datasheet, there is a specification for the core current (Ivdd) and current for each output (Ivddo[n]), spec'd at Vddo at 3.3V and 2.5V.

If I'm running the device with Vddo = 1.8V, can I assume the current will change linearly? Ex: The core current will be 16mA.

Thanks,

Arthur Huang