Part Number: CDCE706
Other Parts Discussed in Thread: CDCM6208V1
I need to generate two in-phase differential clocks from a single input reference clock. My two outputs are 100Mhz and 10Mhz. The maximum input reference clock I can source is 25Mhz, which means I need to both multiply and divide the input, i.e. multiply by 4 and divide by 2.5. The CDCE706 can generate the two frequencies but it appears to be able to output only one clock at a time.
Does anyone know if the CDCE706 can output two different frequencies, in-phase and simultaneously?
If not, if there another device I can use?