Hello,
I use a TLC555 as a monostable. In the worst case, when I take into account the TCR (15%) and tolerance (10%) for capacitors X7R, this monostable shall provide a pulse with a duration between 3.65s and 6.2s. In some case, at ambient temperature, I measure a pulse higher than 6.2s (about 6.5s or 6.7s). anybody can help me understand why or Do you know if anybody already has a similar problem? already meet an equivalent problem.