Part Number: LMK04616
Other Parts Discussed in Thread: LMK04832
I would like to use the LMK04616 in a multi-chassis system, and synchronize them so a SYSREF signal in one chassis is synchronized to a SYSREF signal in a second chassis. My plan would be to distribute a copy of a reference clock to each chassis, taking care to equalize the phase at each chassis (or calibrate within the chassis for any phase difference). In each chassis the LMK04616 would be in dual PLL mode, receiving the reference clock at a CLKin pin. Can multiple LMK04616 ICs be synchronized in this way? If so, what constraints are required in selecting frequencies for reference clock, VCXO, SYSREF, and Device Clk?
I read the SNAU222 Multi-Device synchronization with the LMK04616, but it only discusses multiple devices on the same board.
I see how multiple LMK04832 devices could be synchronized as above if the reference clock is a submultiple of the SYSREF (because CLKout6 or CLKout8 are available at the feedback MUX of the first PLL). I don't see how to accomplish the same in an LMK04616, unless all dividers can be sync'd on an edge of the CLKin signal or an edge of the PPL1 phase detector input. The LMK04616 does not allow an output to feedback to the first PLL.