This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODELOADER: LMK4803B Ext VCO setting

Part Number: CODELOADER


I have a problem with a CodeLoader LMK4803B configuration. In following image the output frequency seems to be correct. Mode selects the Internal VCO of 2000MHz for CLKout0_1 and divided by 10 gives 200MHz on CLKout0.

But now by changing the mode to "Dual PLL, Ext.VCO (Fin)" I think the selected frequency should be the frequency on CLKin, which is 100MHz. So I expect the CKLout0 to change to 100MHz/10 = 10MHz, but it is stuck on 200MHz. Do I misunderstand the meaning of the Mode setting or is it a configuration issue?

I attached the settings file for CodeLoader. I hope you can help me with this problem.

Thank you

Josh

[SETUP]
ADDRESS=888
CLOCK=4
DATA=2
LE=6
PART=LMK04803B
PINPOSITION00=1
PINPOSITION01=7
PINPOSITION02=5
PINPOSITION03=10
[MODES]
NAME00=R0 (INIT)
VALUE00=131072
NAME01=R0
VALUE01=1311040
NAME02=R1
VALUE02=2148795009
NAME03=R2
VALUE03=2148794626
NAME04=R3
VALUE04=3222536227
NAME05=R4
VALUE05=2148794436
NAME06=R5
VALUE06=2148794405
NAME07=R6
VALUE07=101056518
NAME08=R7
VALUE08=1610612743
NAME09=R8
VALUE09=65544
NAME10=R9
VALUE10=1431655753
NAME11=R10
VALUE11=268583242
NAME12=R11
VALUE12=468758539
NAME13=R12
VALUE13=185335916
NAME14=R13
VALUE14=320070221
NAME15=R14
VALUE15=3539992590
NAME16=R15
VALUE16=2147516431
NAME17=R16
VALUE17=3243574288
NAME18=R24
VALUE18=88
NAME19=R25
VALUE19=46661657
NAME20=R26
VALUE20=2947022874
NAME21=R27
VALUE21=469762395
NAME22=R28
VALUE22=2097500
NAME23=R29
VALUE23=25166173
NAME24=R30
VALUE24=33554782
NAME25=R31
VALUE25=2566917407
OSCIN00=100
EXTRA_PLL_N_DIV_1_00=1
OSCIN01=100
EXTRA_PLL_N_DIV_1_01=1
PINS=1
[BURST]
COUNT=0
[FLEXHASH]
HASHVALUE=0