I'm trying to program a LMK03328 on a different board using the LMK03328-EVM by connecting the I2C of the EVM to an I2C at the other board.
I have established connection and I can config. the device on the other board using the TICS-Pro as a slave address different than the one on the EVM.
But as I tried to program the EEPROM by pressing first: (2) Write GUI Map -> SRAM, and after that: (3) Program EEPROM <- SRAM , I get the message
"EEPROM_Program...done", with no really EEprom programing (If I switch off the board and turn it on the LMK03328 does not establishes any clock). Is there a switch or
something else I should do in order to program the EEPROM on this configuration ?