Part Number: CDCE62002EVM
Hello.
I need to generate a 45MHz clock through CDCE62002EVM. I selected AUX as Input source frequency. I used frequency planner to set the dividers for output of 45MHz. I am not getting any output.
In the GUI, the indicator for Lock, EVM Power, USB Status, and SPI Bus Status are on. However, the PLL LOCK LED indicator on the board is off. All LED on the board except the PLL are on.
There is no output frequency.
See below for register values.
REGISTERS
0 F5D800A0
1 A384E001
2 60002A12
PORTS
0 DD
1 FF
2 DF
3 F9
INPUTS
PRI 25
AUX 25
EXTERNAL COMPONENTS
C4 925.3496n
R4 105.7999
C5 15.1123n
Regards
Jungkeun Park