Part Number: CDCLVC1310
Other Parts Discussed in Thread: LMK00101, LMK00105
Hi Team,
How are the four pins VDDO map to the output channel 0~9 ? If one of the VDDo pin no power, which output channel will be influenced?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CDCLVC1310
Other Parts Discussed in Thread: LMK00101, LMK00105
Hi Team,
How are the four pins VDDO map to the output channel 0~9 ? If one of the VDDo pin no power, which output channel will be influenced?
Thank you.
Hi Alan,
My question is in some case, one of the VDDO pin no power, but other 3 pins work normally. The outputs will be effect or not?
Thanks.
The VDDOs pins are bonded onto a VDDO power ring on the die, so the pins are all connected together internally. All outputs should remain active when only one VDDO pin is unpowered.
Alan