This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04832: PLL2 Will Not Lock

Part Number: LMK04832
Other Parts Discussed in Thread: ADS42JB69EVM, LMK04828

Hello, I am having trouble getting PLL2 to lock on the LMK04832. Some background info :

  • The part is installed on an ADS42JB69EVM
    • The LMK04828 that was originally on the board was removed and replaced with the LMK04832
    • Configuration registers are programmed via SPI, we are not using the ADS42JBxx EVM GUI

  • We are using the onboard 100 MHz oscillator
  • PLL1 NCLK Mux is set to use OSCin
  • PLL1 N Divider is set to 100
  • PLL2 reference frequency doubler is disabled
  • PLL2 reference clock mux is set to use OSCin
  • PLL2 reference clock divider is set to 1
  • VCO mux is set to VCO0
  • PLL2 N prescaler is set to 5
  • PLL2 NCLK mux is set to use PLL2 prescaler
  • PLL2 N clock divider is set to 5
  • PLL1 LD is set to PLL1 DLD, push-pull output
  • PLL2 LD is set to PLL2 DLD, push-pull output

I observe that the LMK_LOCKED LED (driven by STATUS_LD1) is on, but the PLL2_LOCKED LED (driven by STATUS_LD2) remains off. The PLL2_LOCKED LED does turn on if I set the PLL2_LD_MUX to use PLL1 DLD, so the LED itself does work.

Are there any suggestions for other registers to look at or things to try next?

Thank you,

Branden