Part Number: CDC3RL02
Hi team,
I have a question regarding CDC3RL02. Here is my basic setup:
- VBATT = 3.3V
- MCLK = 24MHZ 1.8V CMOS
- LDO = unused/floating
With the above, my output looks like Image 1 (below). However, when I drop VBATT to 1.8V, the output looks like Image 2 (below)--it cleaned up quite a bit. So I have two questions:
- Can I operate at VBATT = 1.8V - are there any potential long-term problems with that approach? This isn't within spec according to the datasheet, but the results look better.
- Is my problem potentially related to the floating LDO? Does the LDO need to be connected to a within-spec capacitor even if it's unused?
Bonus third question - is there anything else that might be causing this problem? Thanks in advance for your help!
1. Output when VBATT = 3.3V (bouncing back and forth between 3.3V and 1.8V)
2. Output when VBATT = 1.8V
Regards,
Brian Angiel