Part Number: LMK04828BEVM
Other Parts Discussed in Thread: CODELOADER, LMK04828, LMK04803,
Hello,
I have problems setting up the evalkit. I need the device for a clock distribution of 38.4MHz to at least 6 outputs.
Used Software is Codeloader 4, because i can't find the Tic's Pro Software anywhere.
Now when I'm Powering up the board and connect it with the Usb2Any-device i can access the Configuration.
I've tried the default mode with 122.88MHz first and just wanted to configure all the Outputs to be at the same Phase. But with the delay options avaiable i can't do more than 5 to ten degrees change.
Also there is a problem with the Powerlevels. I've activated 4 Chanels at once and set them all to lvpecl16, but on the oscilloscope they all have different Levels.
What do I do wrong ? Is there any document about the Software and how to use it or the Evalkit and how to set it up for different usecases?
As I said I just want to have a 6-output 38.4MHz clkock with all channels in phase
kind regards
Raffael