Part Number: LMX2595
Other Parts Discussed in Thread: PLLATINUMSIM-SW
1. What is the switching speed between to toggle between frequency to another?
2. What setting or approach will aid in reducing the switching speed? i.e. VCO setting, etc.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMX2595
Other Parts Discussed in Thread: PLLATINUMSIM-SW
1. What is the switching speed between to toggle between frequency to another?
2. What setting or approach will aid in reducing the switching speed? i.e. VCO setting, etc.
Stephanie,
This switching time is the sum of the VCO calibration time and the analog settling time, which both depend on the application. The VCO Calibration time is on the order of 50 us, but can be sped up and depends on the OSCin frequency. The analog settle time depends on the loop bandwidth. To speed up the VCO calibration time, we offer partial assist and full assist modes, and these are described in the datasheet.
I also encourage you to download our PLLatinum Sim tool at ti.com/tool/PLLATINUMSIM-SW
This tool simulates both VCO calibration time and analog settling time.
Regards,
Dean
Hi Dean,
Will switching frequency within the same VCO core assist in reducing the re-calibration time?
For instance, VCO1 is selected and calibrated for 7.6GHz. What would be the switching speed to toggle to 8GHz, within the same VCO1 core? Or will the VCO have to be re-calibrated every time a frequency is changed?
Regards
Stephanie