Hello,
We are currently evaluating the CDCEL913 for use in one of our designs and are interested in the spread spectrum clocking feature. We've got the CDCEL913PERF-EVM evaluation module and SSC is working just fine. However, section 9.2.1 of the datasheet makes specific references to a couple of modulation control parameters that I cannot find further details for. Specifically, the modulation frequency and shape. I see no reference to these parameters in the Clock Pro software, nor the device registers. Is this a documentation error or can I hopefully just twiddle some undocumented register bits? Does anyone have any feedback or experience with these features? If it's relevant, we're planning on controlling the part via I2C.
Thanks for your time.