This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571: LMX2571 No Modulation

Part Number: LMX2571

I have tried programming the LMX2571 so that it is in FSK I2S mode, and it seems that i am sending data correctly to the device.  The carrier signal is created and accurate, but clocking in data doesn't output any modulation.  I have set FSK_MODE_SEL1 to 1, FSK_MODE_SEL0 to 0, and FSK_EN_F1 to 1 as the data sheet describes for setting to I2S mode.  I am sending data (16 bits) on the low side of the frame and have set FSK_I2S_FS_POL correctly based on that as well, but it seems that I am missing something in the set up still.  Is there something I am maybe over-looking in the set up of this device?