Other Parts Discussed in Thread: TINA-TI, , TL494
Tool/software: TINA-TI or Spice Models
Dear Sir/Madam,
I am designing a PWM generator using a NE555 timer in order to drive Half Bridge (which has both high side and low side switching). I have designed a circuit which gives non-inverting PWM signal using NE555 and I have added the common-emitter to get the inverted PWM to drive low side switch.
I am facing an issue, how this non-inverting PWM signal is used to drive the high side switch with differential potential and I went through some of the analog design circuits for half bridge driver but failed to understand.
Specifications:
- The input to the NE555 timer is 5V (TTL)
- The input to the half-bridge circuit is 15V
I request an expert to answer my question
Thank you in advance,
Swetha Revanna