Part Number: LMX2572LP
Tool/software: WEBENCH® Design Tools
Hi.
I'll would like to use the LM2572 to generate a fixed oscillator at 1030MHz using a 10MHz reference. My first idea is using a 103 divider to work at 10MHz at frequency detector. I'm triying to evaluate the phase noise performances of LM2572 using the TLPLLPlantimum SW, but when I select the configuration showed in the figure, the box for the output frequency at the fvco and the output is on red. Could it be possible to use this part in this configuration? or we have to generate a higher frequency at the internal VCO and use the divider to get the final lower frequency. I have tryed to attach the .sim file and the phase noise reference characteristics but it couldn't make it so I put a picture with a screen capture.
Thanks in advance.