Part Number: LMK04610EVM
Other Parts Discussed in Thread: LMK04610
Hi!
In the LMK04610 EVM you decouple the supply pins of the LMK04610 with ferrite beads and 10 uF and 0.1 uF ceramic capacitors - L5, C113, C115 for VDD_CORE; L7, C121, C123 for VDD_PLL1 and so on for every supply pin (see SNAU201A – January 2017 – Revised February 2017, page 25).
Such a configuration forms a hi Q LC-circuit, i.e. the voltage on the corresponding supply pin will oscillate in response to rapid changes of the current flowing through the pin.
Are the currents through the supply pins of the LMK smooth enough not to cause the decoupling circuit to oscillate or perhaps this effect is not important enough to be considered? Would it be more robust to replace 10 uF ceramic capacitors in the current configuration with 10uF tantalum with certain esr to lower the Q or to add bulk tantalum capacitors to the current configuration to damp out any resonance? Is it a good practice to use ferrite beads with low esr ceramic capacitors without any damping?
Thanks in advance!
Best regards, Vic.